alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon
Nordival - Swagelok Italia

Your Authorized Swagelok Sales and Service Center

How to Reach Us

Locate us on google maps. 

our address is:

NORDIVAL Srl

VIA STREPARAVA CAV. LAV. ANGELO LUIGI, 1 
25038 ROVATO (BS)


ROVATO is located in an area called Franciacorta, by the oriental slope of Monte
Orfano, 20 km from BRESCIA and 60 km from MILAN and
Road connections are quite easy:

ROVATO, is crossed by the state highway n° 11 Padana Superiore, and it is easy
reachable via TORINO-TRIESTE highway (A4), accessible from Rovato pay tool.

In addition ROVATO is also the seat of a railway station on Milan-Venice line.

BY CAR:
- From A4 highway, take ROVATO exit.
- Just after the pay tool, turn right following direction “Cazzago San Martino”
- Take the first exist off the roundabout,still following direction “Cazzago San Martino”.
- Once in front of the “Bronze wheel” take the first exit to the right (way to Rovato
center) along the overpass.
- Go ahead for approx. 200 mt up to ROVATO road sign.
- At the roundabout take the second exit and straight to Monte Grappa street.
NORDIVAL IS A LITTLE BIT AHEAD ON THE RIGHT SIDE OF THE STREET.
BY AIRPLANE:
  
ORIO al SERIO in Bergamo is the nearest national and internationational airport
located at 33 km from ROVATO
For direct intercontinental flights, MILANO/MALPENSA air terminal is located
at 117 km from Rovato